How to get rid of include statement

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to get rid of include statement

883 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by riscy00 on Tue Dec 24 03:31:23 MST 2013
I was working on a project using version 5 LPCexpresso for LPC1768 and then project suspended for 10 month until now.

I have installed most recent version 6 LPCexpresso package, so I can continue work to finish off.

Attached is the image of the problem. How to get rid of the redundant library which is greyed out.

I tried clear autodiscovery (C/C++ Build/Discovery Options and click "clear" button. This does not remove include statement (from old LCPexpresso).

I cannot delete from the list as shown in the picture, the "Delete" button is greyed out.

The code complies just fine without error/warning reporting.




0 项奖励
回复
1 回复

858 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Dec 24 03:37:28 MST 2013
Take a look at this FAQ. Following the instructions should fix the problem
http://www.lpcware.com/content/faq/lpcxpresso/invalid-project-path-warnings
0 项奖励
回复