Content originally posted in LPCWare by riscy00 on Tue Dec 24 03:31:23 MST 2013
I was working on a project using version 5 LPCexpresso for LPC1768 and then project suspended for 10 month until now.
I have installed most recent version 6 LPCexpresso package, so I can continue work to finish off.
Attached is the image of the problem. How to get rid of the redundant library which is greyed out.
I tried clear autodiscovery (C/C++ Build/Discovery Options and click "clear" button. This does not remove include statement (from old LCPexpresso).
I cannot delete from the list as shown in the picture, the "Delete" button is greyed out.
The code complies just fine without error/warning reporting.