How to get LPC1114 in programmable state

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to get LPC1114 in programmable state

783件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by faizal on Fri Jun 24 06:53:35 MST 2011
Hello,

Im programming LPC1114. When i tried to debug,i got error said that :

Failed on connect: Ee(07) Bad ACK returned from status-wire error.:(

Does this means that my debug connection is damaged?
0 件の賞賛
返信
2 返答(返信)

772件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by faizal on Fri Jun 24 08:07:20 MST 2011
Thanks a lot Zero, u are my saviour. It was because i connected P0_10 to a wire. I followed the instruction to get debug access and now it works just fine. Again,thanks.:)
0 件の賞賛
返信

772件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Fri Jun 24 07:08:25 MST 2011
Are you using your own board or LPCXpresso?

Try: http://support.code-red-tech.com/CodeRedWiki/DebugAccessChip

If you are trying to connect a new board via SWD I would suggest to check your SWD / Reset /  Power connection.

See also:

http://knowledgebase.nxp.com/showthread.php?t=1637

http://knowledgebase.nxp.com/showthread.php?t=1822
0 件の賞賛
返信