How to debug about LPCXpresso?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to debug about LPCXpresso?

980 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Andy Yang on Fri Aug 23 01:34:21 MST 2013
Hi,everyone:
I'm new in this area and I use LPCXpresso IDE in some time ago.
It's my first topic in this forum.thinks.
now,when I try to debug my project,it always shows this error information as below:
[img]sfa[/img][img=370x150]D:\1.bmp[/img]

(ps:code runs OK,while debug is unsuccessful...)

at last,I download some sample code on websit and then debug, Still have problems:
[img=630x358]D:\2.bmp[/img]

(ps:I used to develop project by using Keil MDK,in Keil environment,I can debug project via virtual simulation simply.)

If I disconnect target,Can I debug project use virtual simulation?
By the way,how can I debug project corrocttly? What should I change some setting or configration?
Who can provide me some advise?
Look forward to your reply.



0 Kudos
Reply
2 Replies

916 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Andy Yang on Sun Aug 25 02:00:06 MST 2013

Quote: lpcxpresso-support
Your images have not appeared and so we do not know what error your are receiving and therefore cannot help. Please repost the image and also provide the text of the error message.




Thank you very much.

Now,I meet some problems when I try to upload the images. I ready to provide the detailed information about error windows.
In order to solve this problem better.I list operation process:(LPCXpresso vision: v5.2.4)

step 1:Creat a new project and named "MyProject".(OK)

step 2:Edit code and compile it.(OK)
       (output"*.hex" file and "*.axf"file correctly)

step 3:Download "*.hex" file to the target board.(OK)
       (use Magic tool,ISP mode)

step 4:Debug part.
       "QuickStart"-"Debug and Run"-"Debug 'MyProject'[Release]"
       After I click "Debug 'MyProject'[Release]",a information window named 'problem occurred' shows on screen,it says:
       'Launching MyProject' has encountered a problem.An internal error occurred during: "Launching MyProject".java.lang.NullPointerException

      The console window shows:'make: Nothing to be done for `all'.'

I hope that what is said above can help you understand my problem. Now,I don't know what can I do.
If I do not connect target board,Can I debug project use virtual simulation?
Do I need to change some settings?

regards.
0 Kudos
Reply

916 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Aug 23 03:06:47 MST 2013
Your images have not appeared and so we do not know what error your are receiving and therefore cannot help. Please repost the image and also provide the text of the error message.
0 Kudos
Reply