Help to find the headers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Help to find the headers

1,376件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rezaabdi on Thu Aug 15 05:48:55 MST 2013
Hi
I'm looking for 2 header (cr_section_macros.h And  NXP/crp.h)
If friends have access to the header
If possible upload them to the
Thanks...
0 件の賞賛
返信
5 返答(返信)

1,296件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rezaabdi on Thu Aug 15 08:47:04 MST 2013
thank you
I did not know
Do you know of another way?
But I'm working Keil
0 件の賞賛
返信

1,296件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Aug 15 08:40:28 MST 2013
neither of these files is applicable to Keil - they are only for LPCXpresso.
0 件の賞賛
返信

1,296件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rezaabdi on Thu Aug 15 08:01:35 MST 2013
oh
im sorry
I was not looking for the exact address
I do not have this software LPCXpresso_5.2.6
I noticed the wrong address and now I'm taking the Keil Program
If you could help
Thank you
0 件の賞賛
返信

1,296件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rezaabdi on Thu Aug 15 07:23:58 MST 2013
Thanks for the answer
I looked Directions
C:\nxp\LPCXpresso_5.2.6\lpcxpresso\tools\arm-none-eabi\include\NXP\crp.h
C:\nxp\LPCXpresso_5.2.6\lpcxpresso\tools\arm-none-eabi\include\cr_section_macros.h
But the files are not available
Thanks if you can help me!
0 件の賞賛
返信

1,296件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Paul on Thu Aug 15 07:15:13 MST 2013
If you have LPCXpresso installed in the default location, you should be able to find these header files in the following directories:
C:\nxp\LPCXpresso_5.2.6\lpcxpresso\tools\arm-none-eabi\include\NXP\crp.h
C:\nxp\LPCXpresso_5.2.6\lpcxpresso\tools\arm-none-eabi\include\cr_section_macros.h
If you cannot find them, let us know.
0 件の賞賛
返信