Help select controller for CAN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Help select controller for CAN

796件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by prancius on Mon Sep 10 03:39:48 MST 2012
Hello,

I am woning with PIC controllers and new in NXP.
I my device i want implement CAN option.
As i see NXP controller have built in transceiver and i would like to start with NXP.

Can you recomend what controller i should use for CAN project?

Thank you
0 件の賞賛
返信
1 返信

790件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Mon Sep 10 03:44:45 MST 2012

Quote: prancius
As i see NXP controller have built in MCP2551...

NOOOOOOOOOOOOOOO :eek::eek:

NXP doesn't build in microchip :)


Quote: prancius
...i would like to start with NXP.



Easiest way to start is LPCXpresso11C24:

http://www.embeddedartists.com/products/lpcxpresso/lpc11C24_xpr.php

with CAN transceiver included ;)
0 件の賞賛
返信