Getting LPC1347 USART to work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Getting LPC1347 USART to work

1,019 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by zmogedra on Thu Feb 14 13:22:23 MST 2013
Hi, I have just started USART project and I have some questions.
1. There are different pins noted RXD TXD on LPC chip that means if you only have 1 usart but you can choose on which pair of pins?
2. Is by default protocol asynchronous?
3. Should I follow UART protocol like the one given in LPC11xx examples?

Maybe someone has an example of lpc1347 usart (asynchronous), because I can't seem to find it on the internet?

ThankYou.
0 Kudos
Reply
2 Replies

962 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by zmogedra on Sun Feb 17 06:52:51 MST 2013
Yeah thanks, managed to power it up and make it work.
0 Kudos
Reply

962 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Feb 14 13:55:52 MST 2013

Quote:

1. There are different pins noted RXD TXD on LPC chip that means if you only have 1 usart but you can choose on which pair of pins?

Yes, you can. Of course you have to select correct I/O configuration for this pins ;)


Quote:

2. Is by default protocol asynchronous?

Bit SYNC of SYNCCTRL is Reset by default :eek:


Quote:

3. Should I follow UART protocol like the one given in LPC11xx examples?

Why not :confused:
0 Kudos
Reply