Generating Intel Hex Files

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Generating Intel Hex Files

1,228件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ktownsend on Wed Dec 16 16:12:41 MST 2009
I'm not sure how relevant this is to other people, but since we only have x64 machines setup in the office we're currently unable to use the LPC-Link (I'll probably setup a virtual machine for this when I can find the time).  If you want to be able to transfer your compiled code to a board using FlashMagic you'll need to configure LPCXpresso to build an [B]Intel Hex file[/B] as well.  We've put together a simple tutorial showing how to do that if anyone comes across the same situation/need themselves:

http://www.microbuilder.eu/Blog/09-12-16/Building_Intel_Hex_Files_with_LPCXpresso.aspx
0 件の賞賛
返信
3 返答(返信)

1,196件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_USA on Tue Jan 05 16:00:20 MST 2010

Quote: cole
I would like to see a 64-bit Windows 7 driver soon.  I just got an LPCXpresso LPC1114 board in a few days ago, but I do not have any 32-bit systems in my lab (I haven't had a 32-bit system in several years!)..

Additionally, Linux support would be good.  I am surprised how often Linux is overlooked as a powerful and popular development environment.

Thanks,
-Chris



Hi Chris, we expect to release 64-bit Windows drivers this year, however a specific date is not available yet.

Regarding Linux, although the LPCXpresso environment is not available on Linux, it should be possible to use standard open-source tools such as Eclipse and GCC and flash the LPCXpresso MCU with the on-chip UART ISP and USB ISP features.

Thanks,
-NXP
0 件の賞賛
返信

1,196件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cole on Sat Jan 02 20:53:57 MST 2010
I would like to see a 64-bit Windows 7 driver soon.  I just got an LPCXpresso LPC1114 board in a few days ago, but I do not have any 32-bit systems in my lab (I haven't had a 32-bit system in several years!)..

Additionally, Linux support would be good.  I am surprised how often Linux is overlooked as a powerful and popular development environment.

Thanks,
-Chris
0 件の賞賛
返信

1,196件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_USA on Thu Dec 17 08:59:32 MST 2009
We are working on creating 64-bit drivers for LPC-LINK. In the intervening time, is it possible to use Windows XP mode in Windows 7 to run LPCXpresso? It is basically a VM already set up.

-NXP
0 件の賞賛
返信