GPIO interrupt not working on LPC1769

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPIO interrupt not working on LPC1769

2,254件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by DjCracks on Tue Nov 06 13:08:37 MST 2012
I've been using the GPIO interrupts for a sumo bot I'm building but when I connect the motors the interrupts activate alone. I suppose it is because of some kind of magnetic field the motors are producing. Does anyone know how to solve this?

Thank you.
0 件の賞賛
返信
10 返答(返信)

2,209件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fjrg76 on Fri Nov 09 12:43:26 MST 2012
In hardware:

Try to implement a passive RC filter in the uC inputs

In software:

Implent debouncing techniques:
a) Measure the time that the input is in its active state, say low-level. If such a level lasts for at least n cycles, then the inputs is taken as a correct one; otherwise it's discarded.

b) Poll the input and count the different levels, and after some time take as valid input the one that has the majority.
0 件の賞賛
返信

2,209件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Nov 08 11:47:54 MST 2012
As mentioned already 2 days ago: chokes as shown in figure 23 of http://cache.freescale.com/files/microcontrollers/doc/app_note/AN2764.pdf ;)
0 件の賞賛
返信

2,209件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by DjCracks on Thu Nov 08 10:48:19 MST 2012
The problem after some tests is this: when I disconnect the sensors from the LPC the interrupts don't activate by themselves but when I connect the cable they do. I've installed a 1k pullup resistor and it's still the same. Now I'm using a shielded cable and some caps to filter and they improved a little bit but still don´t work fine. The motors are definetley introducing noise in the cables. Does anyone know some workaround?

Thanks.
0 件の賞賛
返信

2,209件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fjrg76 on Wed Nov 07 18:53:55 MST 2012

Quote: DjCracks
I do know what a pullup resistor is. Is it necessary (even though I set the input as Tristate and it is just receiving the signal of a phototransistor from a CNY70 sensor) to add a pull up resistor?



Normally a phototransistor doesn't include a pull-up resistor in its output. Besides, it's said (somewhere) in the user manual that the internal pull-up resistors inside the uC are not intended to be as general purpose ones. So, in a noisy enviroment it's better off you use a strong pull-ups.
0 件の賞賛
返信

2,209件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by graynomad on Wed Nov 07 18:40:06 MST 2012
Do you have the input on the collector of the sensor?

If so then when there is no reflection the transistor is off and the input is floating. You should [B]never [/B]have a floating input so yes I'd say you need the pullup.
0 件の賞賛
返信

2,209件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by DjCracks on Wed Nov 07 18:29:00 MST 2012

Quote: graynomad
Presumably you know what a pullup resistor is, normally you use 10k or even up to 100k but I would suggest "strong" is more like 1k.


I do know what a pullup resistor is. Is it necessary (even though I set the input as Tristate and it is just receiving the signal of a phototransistor from a CNY70 sensor) to add a pull up resistor?
0 件の賞賛
返信

2,209件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by graynomad on Wed Nov 07 16:41:23 MST 2012
Presumably you know what a pullup resistor is, normally you use 10k or even up to 100k but I would suggest "strong" is more like 1k.
0 件の賞賛
返信

2,209件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by DjCracks on Wed Nov 07 14:26:29 MST 2012
We are using fast diodes (free-wheel) but I don't know what you mean by strong pull-up resistors in the inputs. Could you clarify this for me?

Thanks
0 件の賞賛
返信

2,209件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fjrg76 on Tue Nov 06 22:34:14 MST 2012
Free-wheel diodes? Strong pull-ups in inputs?
0 件の賞賛
返信

2,209件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Tue Nov 06 13:20:16 MST 2012
Just a guess: Some kind of EMC protection :confused:

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN2764.pdf
0 件の賞賛
返信