GDB question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GDB question

723件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by micronpn on Mon Jun 21 07:44:05 MST 2010
I daily use LpcXpresso to develop on NXP microcontrollers and sometime it is useful to compile/debug with GCC/MinGW without the hardware fo debug internal functions without flashing the microcontroller. Also if  I was able to use MinGw directly under LLpcXpresso, I would prefer to use a standard Eclipse CDT installation. With a big surprise I see that under LpcXpresso I can debug stdin/stdout directly on a Win/Dos console instead std Eclipse/CDT doesn't open che Win/Dos console and the eclipse console (as in LpcXpresso also) doesn't work in input and visualize the output only after program exit. So... the question: did you personalize LpcXpresso to solve the console problem or is it just a different setup that I have to copy?
0 件の賞賛
返信
1 返信

717件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Jun 22 01:36:08 MST 2010
I'm sorry, but I don't understand the question. Can you explain in more detail what you are trying to do?
0 件の賞賛
返信