FreeRTOS redlib or newlib

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FreeRTOS redlib or newlib

894件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tridentsx on Fri Oct 07 12:03:46 MST 2011
I have started a project using LPCXpresso and EA LPC1769 board, so far so good I reused the code from the code red freertos example. I noticed that there examples uses newlib by default, why is that ?

Are there issues with redlib and FreeRTOS ?

Regards /// Carl
0 件の賞賛
返信
1 返信

811件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by DaveNadler on Fri Oct 07 15:04:46 MST 2011
[FONT=Arial]I'm using RedLib with FreeRTOS 7 on LPC1114, its AOK.
Make [U][B]sure[/B][/U] you get latest version of FreeRTOS from the
FreeRTOS web site for real work...
Hope that helps,
Best Regards, Dave[/FONT]
0 件の賞賛
返信