FreeRTOS + IO for the CAN Peripheral

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FreeRTOS + IO for the CAN Peripheral

797 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by niharika_singh on Mon Nov 25 09:54:04 MST 2013
Hi,

I recently finished Post graduate diploma course on Embedded Systems. As a part of our course we had to come up with a project during the last month.
I decided to add support for the CAN peripheral in the FreeRTOS + IO architecture. I made changes in to the source code of FreeRTOS + IO so that the CAN peripheral could be accessed via POSIX-like open(), read(), write() and ioctl() calls. I was able to manage the basic CAN communication between between two microcontrollers using the driver I wrote but due to short of time I could not much CAN features in the driver code.

I have some free time on my hands now so I am looking more into this project again but I have a few doubts about the transfer modes used with FreeRTOS + IO architecture. Which transfer mode should be the best to use with CAN protocol?
Also as CAN is a much bigger protocol than SPI or I2C, so I want suggestions, as what all features should be included in the driver and which can be done away with?

Thanks and regards,
Niharika

0 Kudos
Reply
1 Reply

758 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Nov 26 02:47:34 MST 2013
You might do better posting this question to the FreeRTOS forum…

http://sourceforge.net/p/freertos/discussion/382005/

Regards,
LPCXpresso Support
0 Kudos
Reply