Free edition maximum build size

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Free edition maximum build size

575件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by askar on Thu May 15 22:57:57 MST 2014
Hi,

I am using Lpcxpresso free edition 7.0.0-92 in a workspace that uses multi core applications for LPC4357.
a project for M4 and another one for M0 are used. the document says that maximum build size
for a target is 256 KB.
does this mean that maximum size for M4 is 256KB and maximum size for M0 is 256KB?
and we indeed can build maximum 512KB for a multi core application?

Best Regards,
Askar
0 件の賞賛
返信
1 返信

565件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri May 16 00:36:45 MST 2014
The *build* size is unlimited. It is the *debug* that is restricted.

Debug is restricted to a download AND a debug limit of 256k in total.
0 件の賞賛
返信