Flash driver "ProgramPage" return code: 0x9

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Flash driver "ProgramPage" return code: 0x9

641 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by IanB on Sat May 30 04:11:59 MST 2015
Could somebody please tell me what this error means.

I clicked "help on this error" and got the attached. Not much help there, then?
0 项奖励
回复
3 回复数

622 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by IanB on Mon Jun 01 12:14:39 MST 2015
The problem was rather more of a comedy of errors. The green "debug" icon was not compiling the project that I thought it was, and the result is that it was trying to put the program for an LPC1112 into an LPC812.

However, I do think that an error message that said "Device signature does not match" would have taken me to the cause of the problem in minutes rather than hours.

0 项奖励
回复

622 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Jun 01 00:09:11 MST 2015
As per the comment from 1234567890, please post details of your setup including LPCXpresso version and debug probe, target MCU and board, what you were doing when you saw the error, and also the full debug log.

http://www.lpcware.com/content/faq/lpcxpresso/debug-log

It would also be helpful to understand whether you have been able to successful program before or not?

Regards,
LPCXpresso Support
0 项奖励
回复

622 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by 1234567890 on Sat May 30 09:14:09 MST 2015
Details about chip, IDE, hardware, software, occurrence/time of the message and so on could be very helpful...

A shot in the dark: See attachment.
0 项奖励
回复