Flash-Tool in GUI locks up on Mac

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash-Tool in GUI locks up on Mac

585件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sravet on Thu Jan 03 21:01:06 MST 2013
I am using FlashTool (the chip icon in the GUI) to download .bin and .axf files to both an LPCxpresso LPC1114 board and to a custom board with LPC1768.  All of these have the same behavior:  I select the file, verify the proper CPU architecture, then click OK and am presented with a progress bar that never progresses.

From the shell I am able to see the command that lpcxpresso uses to flash (crt_emu_lpc11_13_nxp or crt_emu_cm3_nxp), and if I run it manually from the shell then it seems to complete fine.  Not sure what the GUI is waiting on.  in the shell ps -ax shows that the the flash programmer is still running, although if I copy/paste the exact same command to the shell prompt it runs and exits fine.

LPCxpresso version is 5.0.14, and I am running on a Mac.  Any suggestions on how to further debug this?

thanks,
--steve
0 件の賞賛
返信
0 返答(返信)