Firmware installation on LPC1342

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Firmware installation on LPC1342

670 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jedx on Mon Jan 16 06:36:21 MST 2012
It is okay to replace the stock 16kb firmware file of LPC1342 with an 8kb firmware file?

I am developing an Open PCD 2 board and the given firmware file has a size of 8kb file.

TIA.
0 项奖励
回复
1 回复

653 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Mon Jan 16 20:54:15 MST 2012
As user manual describes:

Quote:

The entire available user flash is mapped to a file of the size of the LPC134x flash in the host’s folder with the default name ‘firmware.bin’. The ‘firmware.bin’ file can be deleted and a new file can be copied into the directory, thereby updating the user code in flash. Note that the filename of the new flash image file is not important. After a reset or a power cycle, the new file is visible in the host’s file system under it’s default name ‘firmware.bin’.

It's a little bit confusing that the complete available flash is shown as 'firmware.bin'. But  of course you can delete it and copy your own bin file in there.
Reading flash file next time will show you your new file named 'firmware.bin'. So don't expect to see your original file name and file size :)
0 项奖励
回复