Fibonacci Serie

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Fibonacci Serie

2,435 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cromo1212 on Thu Oct 02 17:00:17 MST 2014
Hi Everybody,
I really need your help on my school gave a homework that is creating a task that develops the fibonacci serie. that needs to save the first 50 numbers and show the first 10 of them (printing each one on one separate row and with 1 sec of delay)

i havent ever work before on this, so can you please help me with this?


it will be really appreciate it.

thanks!!
0 Kudos
Reply
5 Replies

2,420 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Pacman on Mon Oct 06 21:04:30 MST 2014
That's a very nice wiring! :)
0 Kudos
Reply

2,420 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Mon Oct 06 10:18:00 MST 2014
Hi cromo1212,
download lpcopen packages from
http://www.lpcware.com/content/nxpfile/lpcopen-software-development-platform-lpc17xx-packages

Use one of the example code with your tool chain.

For example, you can find UART example for Keil tool chain here.

lpcopen_2_10_keil_iar_nxp_lpcxpresso_1769\applications\lpc17xx_40xx\keil_uvision_projects\nxp_lpcxpresso_1769\periph\periph_uart_rb
0 Kudos
Reply

2,418 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cromo1212 on Sun Oct 05 08:20:22 MST 2014
here is the picture of the LPC.
0 Kudos
Reply

2,418 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cromo1212 on Sun Oct 05 08:18:03 MST 2014
Sure and thanks for your help,
the LPC I am ussing is the LPCXpresso LC1769.
0 Kudos
Reply

2,418 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Fri Oct 03 09:58:00 MST 2014
Hi cromo1212,
Please post  detailed information. Which board are you using? If it is your own board which device are you using?
We have basic example available. It is easy to add this logic.
0 Kudos
Reply