Fatal Error Building Project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Fatal Error Building Project

1,266 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by leon_suburbano on Fri Aug 28 14:03:57 MST 2015
I have a very disturbing situation.

When I try to Build Project [Debug] (My Project is named TP1) I hace a problem and it does not compile.

LOG:

17:45:59 **** Incremental Build of configuration Debug for project TP1 ****
make -r all
Building file: ../src/TP1.c
Invoking: MCU C Compiler
arm-none-eabi-gcc -DDEBUG -D__CODE_RED -DCORE_M3 -D__USE_CMSIS=CMSISv2p00_LPC17xx -D__LPC17XX__ -D__REDLIB__ -I"C:\Users\León\Desktop\CMSISv2p00_LPC17xx\inc" -O0 -g3 -Wall -c -fmessage-length=0 -fno-builtin -ffunction-sections -fdata-sections -mcpu=cortex-m3 -mthumb -specs=redlib.specs -MMD -MP -MF"src/TP1.d" -MT"src/TP1.o" -MT"src/TP1.d" -o "src/TP1.o" "../src/TP1.c"
../src/TP1.c:12:21: fatal error: LPC17xx.h: No such file or directory
#include "LPC17xx.h"
                     ^
compilation terminated.
make: *** [src/TP1.o] Error 1


17:45:59 Build Finished (took 410ms)

Please Help.!!

Oh, the same project has been tried on different computers, but on mine is the problem. I cannot understand, no one have problems with this.

Thanks
0 Kudos
Reply
1 Reply

1,234 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Fri Aug 28 14:24:15 MST 2015

Quote: leon_suburbano
Oh, the same project has been tried on different computers, but on mine is the problem. I cannot understand, no one have problems with this.



Perhaps you are the problem  :O


Quote:
-D__REDLIB__ -I"C:\Users\[color=#f00]León[/color]\Desktop\CMSISv2p00_LPC17xx\inc" -O0 -g3 -Wall -c -fmessage-length=0 -fno-builtin


0 Kudos
Reply