Failed on chip setup: EC(01). Invalid, ....

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Failed on chip setup: EC(01). Invalid, ....

686 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by aadd2000 on Sun Nov 06 05:58:10 MST 2011
Hello,
my LPCXpresso board is broken. Now I bought a new one.
After starting the Debugger I get the error message:

[SIZE=2][COLOR=#008000][SIZE=2][COLOR=#008000]Invalid LPC1114/301 Part ID: 0x2540102B
[LEFT]Known LPC1114/301 ID(s): 0x0444102B[/LEFT]
[/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2][COLOR=#ff0000][SIZE=2][COLOR=#ff0000]03: Failed on chip setup: Ec(01). Invalid, mismatched, or unknown part

[COLOR=black]Can anyone help me?[/COLOR]
[COLOR=black][/COLOR]
[COLOR=black]Andreas[/COLOR]
[/COLOR][/SIZE][/COLOR][/SIZE]
0 Kudos
Reply
1 Reply

661 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Sun Nov 06 06:19:15 MST 2011
Your Debugger is nagging because you've connected the wrong board :eek:

Your board isn't a LPC1114/301 its a (new) LPC1114/302 :)

So just change your MCU setting :rolleyes:

See also: http://knowledgebase.nxp.com/showthread.php?t=1626

and

http://support.code-red-tech.com/CodeRedWiki/ChangingProjectTarget
0 Kudos
Reply