Examples for LPC1347

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Examples for LPC1347

1,880 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Terje on Tue Oct 02 13:03:10 MST 2012
Are there any examples available for LPC1347?
0 项奖励
回复
6 回复数

1,795 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mcembedded on Wed Jan 16 19:31:55 MST 2013
Hi Terje,
ADC example for LPC1347 is available at www.lpcware.com. You can download v1.01 version of the code bundle from
http://www.lpcware.com/content/nxpfile/lpcxpresso-example-projects-and-cmsis-library-lpc131516174546...

Thanks,
NXP Support
0 项奖励
回复

1,795 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cfb on Thu Jan 10 04:18:49 MST 2013
When you purchase an Embedded Artists baseboard you can download the source code for a set of drivers and examples for use with the various peripherals. The Documents and Resources page lists what is included:

http://www.embeddedartists.com/products/lpcxpresso/xpr_base.php

I suspect you'll find everything you need there without having to reinvent the wheel.
0 项奖励
回复

1,795 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CC58 on Wed Jan 09 09:49:29 MST 2013
Not much help.  Alot of sample code is missing.  No ssp.c for SPI.  No adc.c which is ironic since ADC is in file name.  the usb code is very different from 1343.  This doesn't look like it will be easy to port my 1343 code to 1345.  Gonna have to write my own.  Not what I had hoped.
0 项奖励
回复

1,795 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Terje on Thu Oct 04 11:47:12 MST 2012
Thanks, found them.
0 项奖励
回复

1,795 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Wed Oct 03 00:37:10 MST 2012
The LPC1347 examples that ship with LPCXpresso IDE can be found within the examples directory of your installation at:

\Examples\NXP\LPC1000\LPC13xx_12bitADC

[ The "12bitADC" being how NXP wished us to distinguish the 'new' LPC13's from the originals. ]

Regards,
CodeRedSupport
0 项奖励
回复

1,795 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cfb on Tue Oct 02 14:28:27 MST 2012
See the discussion with the subject  'lpc1347 sample codes' in the lpcware lpc13xx forum:

http://www.lpcware.com/forums/microprocessors-forums/lpc13xx
0 项奖励
回复