Example project for AN10955

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example project for AN10955

1,361 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by thinkchip on Tue Sep 07 22:20:13 MST 2010
Is there any example for use the AN10955 for software uart with a timer?
0 Kudos
Reply
4 Replies

1,314 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by thinkchip on Wed Sep 08 20:24:56 MST 2010

Quote: CodeRedSupport
The application note is available from NXP's website at:
http://ics.nxp.com/support/documents/microcontrollers/?search=an10955&Search.x=0&Search.y=0

Download this zip file and unzip it. Inside you will find a PDF of the document itself, together with the example code - including the project ZIP files suitable for use with the LPCXpresso IDE.

Regards,
CodeRedSupport


Thanks a lot, I will try to configure in 9 bit mode data,1 start bit, 1 stop bit, any advice?
0 Kudos
Reply

1,314 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Wed Sep 08 06:24:48 MST 2010

Quote: thinkchip
thanks, but where are this zip files? In what version of lpcxpresso is comming?



The application note is available from NXP's website at:
http://ics.nxp.com/support/documents/microcontrollers/?search=an10955&Search.x=0&Search.y=0

Download this zip file and unzip it. Inside you will find a PDF of the document itself, together with the example code - including the project ZIP files suitable for use with the LPCXpresso IDE.

Regards,
CodeRedSupport
0 Kudos
Reply

1,314 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by thinkchip on Wed Sep 08 05:04:56 MST 2010

Quote: CodeRedSupport
Bit confused as to what you are asking for here. From a quick skim of the apps note it appears to use a timer....



And example projects for use with LPCXpresso are provided. You just need to use the "Import" option in the quickstart panel, and navigate to the LPCXpresso_Soft_UART_1343.zip or LPCXPresso_Soft_UART_1114.zip as appropriate.

Regards,
CodeRedSupport



thanks, but where are this zip files? In what version of lpcxpresso is comming?
0 Kudos
Reply

1,314 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Sep 07 23:32:52 MST 2010
Bit confused as to what you are asking for here. From a quick skim of the apps note it appears to use a timer....


Quote:
This solution relies on a general purpose 32-bit timer and its ability to toggle a dedicated pin while simultaneously monitoring the state of another pin.



And example projects for use with LPCXpresso are provided. You just need to use the "Import" option in the quickstart panel, and navigate to the LPCXpresso_Soft_UART_1343.zip or LPCXPresso_Soft_UART_1114.zip as appropriate.

Regards,
CodeRedSupport
0 Kudos
Reply