Error on connection to LPC1114

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error on connection to LPC1114

1,656 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by FDamn922 on Mon Mar 19 18:21:07 MST 2012
Hi, when I click on Debug and Run -->  Debug 'myProgram' [Debug] button, I get this error:

[I]"Error launching Debug\Myprogram.axf
02: Failed on connect: Ee(07). Bad ACK returned from status - wire error.:"[/I]

I change the usb cable 3 times. But the error persists.
An isolation problem on the usb port of the lpc boar? Is it posible?

(Note: I didn't change any configuration related to oscilator or the system, I just want to turn the led on...)
0 Kudos
Reply
7 Replies

1,649 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vinod on Thu Apr 26 05:32:21 MST 2012
i am using with jtag debugger

Quote: researchinnovation
@FDamn922:-- Hi...!!!

Are you using Baseboard with LPC1114 Emulator or using it alone.
If you are using baseboard also with Emulator then you have to use 2 Nos. of USB cables. One for UART and one for Power. Single Cable would not be sufficient for the power.
If that is not the case then go to "Project" and "Properties" and in "C/C++ Build" Change the "MCU" setting as per your Emulator LPC1114/301/302 etc.
Check the default Jumper settings of the board.

Have patience it will work, Trust me......Just Give a Try.....!!!


Thanks & Regards....:)

0 Kudos
Reply

1,649 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by researchinnovation on Thu Apr 26 05:23:24 MST 2012
@FDamn922:-- Hi...!!!

Are you using Baseboard with LPC1114 Emulator or using it alone.
If you are using baseboard also with Emulator then you have to use 2 Nos. of USB cables. One for UART and one for Power. Single Cable would not be sufficient for the power.
If that is not the case then go to "Project" and "Properties" and in "C/C++ Build" Change the "MCU" setting as per your Emulator LPC1114/301/302 etc.
Check the default Jumper settings of the board.

Have patience it will work, Trust me......Just Give a Try.....!!!


Thanks & Regards....:)
0 Kudos
Reply

1,649 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Apr 26 04:08:20 MST 2012

Quote: vinod
...whatever ur posted it doesnt understood me..



And now I don't understand you :confused:
0 Kudos
Reply

1,649 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vinod on Thu Apr 26 03:23:34 MST 2012
compilation happens without wny error but when it comes to debug &run it gives me the same error,,,
pls help me & whatever ur posted it doesnt understood me..
0 Kudos
Reply

1,649 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pollostar on Thu Mar 22 05:31:12 MST 2012
Replug your connection and wait for couple a minute and try again if it won't work then try
0 Kudos
Reply

1,649 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pollostar on Thu Mar 22 05:30:35 MST 2012
Replug your connection and wait for couple a minute and try again if it won't work then try Technical Support.
0 Kudos
Reply

1,649 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Mon Mar 19 19:08:43 MST 2012
Did you enable 'Vector catch' and switch to ISP already?

http://support.code-red-tech.com/CodeRedWiki/DebugAccessChip
0 Kudos
Reply