Error message - not connect ro emulator!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error message - not connect ro emulator!

513件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by frankwu5 on Wed Jun 09 03:04:55 MST 2010
Hello:

I use the code in my program as below and debug in LPCXpresso environment(LPCXPRESS BOARD - target114).
LPC_IOCON->JTAG_TCK_PIO0_10 &= ~0x07;
LPC_IOCON->JTAG_TCK_PIO0_10 |= 0x02; /* Timer0_16 MAT2 */

I think I use a pin for debugging.

What could I do to recover the porblem? Can I programming any code without dedugging to solve it?

Best Regards,
Frank
0 件の賞賛
返信
0 返答(返信)