Error: No source available for "" (LPC1769, debugging in CodeRed 4.1.0 build 190) )

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error: No source available for "" (LPC1769, debugging in CodeRed 4.1.0 build 190) )

621件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gweppler on Mon Oct 03 03:49:43 MST 2011
I successfully imported and ran/debugged multiple of the examples in LPCXpresso 4.0.6. Debug 'project' allowed me to step through the instructions. At some point, i started to see the error

No source available for ""

When i wanted to start the debug session. I switched workspaces, re-started projects from scratch, even totally wiped 4.0.6 and then re-installed 4.1.0 --- but i keep getting the same error.

I use all default settings - in LPCXpresso as well as in the imported projects.

Any pointers? 

Thanks in advance,
g
0 件の賞賛
返信
1 返信

611件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Mon Oct 03 03:54:38 MST 2011

Quote:
No source available for

Are you trying to debug a library function (=  compiled without debug information) ? That's usually the cause for this message :eek:
0 件の賞賛
返信