Error Launching debug (resource is not open)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error Launching debug (resource is not open)

774 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by E21 on Fri Dec 19 00:11:41 MST 2014
I tried to debug the proyect but I cant becuase of an error  that says:
"Resource /CMSISv2p00_LPC17xx is not open"
[img=1334x634]http://k30.kn3.net/C/F/0/5/A/8/9C4.png[/img]

note: The building has no error.

How can I fix it?
0 Kudos
Reply
2 Replies

751 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by E21 on Fri Dec 19 10:17:06 MST 2014
Thanks, the .project was having problems to be loaded
I created it again and open it

Thanks for the help
0 Kudos
Reply

751 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Dec 19 01:44:41 MST 2014
This means that your project uses CMSISv2p00_LPC17xx, but the project is closed. Open the project and it should work RIght-click on CMSISv2p00_LPC17xx and select Open project
0 Kudos
Reply