Dual Core Project with Hard ABI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Dual Core Project with Hard ABI

940件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by emh203 on Sat Apr 25 12:24:13 MST 2015
Is it possible to setup an LPC43xx dual core project and use HARD ABI on the M4 side?

I have successful compiled all my libraries, etc for project that only uses the M4 core in an LPC43xx with HardABI.   

The problem is that dual core projects merge an M0 binary at the link stage and the linker will always through an error as my M4 configuration uses Hard ABI.

Is there a work around?    

0 件の賞賛
返信
3 返答(返信)

922件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Sun Apr 26 01:39:00 MST 2015
What version of LPCXpresso are you using? As per the notes in the "LPCXpresso IDE latest release" thread, this should work with LPCXpresso 7.7.2.


Quote:
[list]
  [*]Added support for M4 multi-core projects to use HardABI floating point variant
[/list]


Regards,
LPCXpresso Support
0 件の賞賛
返信

922件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Sat Apr 25 15:47:42 MST 2015

Quote: MikeSimmonds
What is "Hard ABI"?



http://www.lpcware.com/content/faq/lpcxpresso/cm4-floating-point
0 件の賞賛
返信

922件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Sat Apr 25 15:37:38 MST 2015
What is "Hard ABI"?

Mike
0 件の賞賛
返信