Dual Core Project with Hard ABI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Dual Core Project with Hard ABI

929 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by emh203 on Sat Apr 25 12:24:13 MST 2015
Is it possible to setup an LPC43xx dual core project and use HARD ABI on the M4 side?

I have successful compiled all my libraries, etc for project that only uses the M4 core in an LPC43xx with HardABI.   

The problem is that dual core projects merge an M0 binary at the link stage and the linker will always through an error as my M4 configuration uses Hard ABI.

Is there a work around?    

0 Kudos
Reply
3 Replies

911 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Sun Apr 26 01:39:00 MST 2015
What version of LPCXpresso are you using? As per the notes in the "LPCXpresso IDE latest release" thread, this should work with LPCXpresso 7.7.2.


Quote:
[list]
  [*]Added support for M4 multi-core projects to use HardABI floating point variant
[/list]


Regards,
LPCXpresso Support
0 Kudos
Reply

911 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Sat Apr 25 15:47:42 MST 2015

Quote: MikeSimmonds
What is "Hard ABI"?



http://www.lpcware.com/content/faq/lpcxpresso/cm4-floating-point
0 Kudos
Reply

911 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Sat Apr 25 15:37:38 MST 2015
What is "Hard ABI"?

Mike
0 Kudos
Reply