Drivers for LPC12xx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Drivers for LPC12xx

1,186件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fjrg76 on Tue Nov 06 14:31:32 MST 2012
Hi,

In this location

C:\nxp\LPCXpresso_4.3.0_1023\lpcxpresso\Examples\NXP\LPC1000\LPC11xx

one can find the file

NXP_LPCXpresso1114-302_2011-02-07.zip

that contains examples and device-drivers for most peripherals found in the LPC11xx uC.

Looking inside in ../LPC12xx folder there isn't a corresponding file for the LPC12xx uC.

Although some drivers can be ported immediatly from LPC11xx to LPC12xx, the latter has peripherals not found in the former.

The CooCox project has device-drivers for the LPC12xx, and they were created for the NXP team, so one might copy them from CooCox to LPCXpresso.

My question is: Is there a similar file containing (official) device-drivers for the LPC12xx in LPCXpresso?

Thank you!!
0 件の賞賛
返信
3 返答(返信)

1,127件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fjrg76 on Wed Nov 14 18:54:38 MST 2012

Quote: fjrg76


The CooCox project has device-drivers for the LPC12xx, and they were created for the NXP team, so one might copy them from CooCox to LPCXpresso.



[SIZE=4][COLOR=Red]WATCH OUT!![/COLOR][/SIZE]

Those drivers don't compile. The drivers themself are great, however, they were taken from another uC (from the same LPC1xxx family, I assume) so a lot of references doesn't exist for the LPC1227 uC.

I've been spending a lot of time porting them (with the correct references) to the LPC1227. Once I finish I'll let them public for those interested in this uC and these drivers.
0 件の賞賛
返信

1,127件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fjrg76 on Tue Nov 06 22:32:26 MST 2012
Thank you for the link, it's gonna be very useful.

Nevertheless, if you look at a LPC1227 project build upon CooCox you'll see a complete device-drivers set for that uC.

Instead of just copying them to LPCXpresso I'd like to know whether is something similar in it. In that fashion the device-drivers will always be up to date according the NXP team.
0 件の賞賛
返信

1,127件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cfb on Tue Nov 06 19:17:29 MST 2012
http://www.lpcware.com/gfiles/devper/lpc12xx
0 件の賞賛
返信