Download/Debug Limit Clarification

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Download/Debug Limit Clarification

783件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by martinmckee on Fri Feb 28 18:54:52 MST 2014
I'm looking to use an LPC4330 in an upcoming application.  In most ways, it is the perfect device for the application which requires both low latency ( which could be handled by the dual core structure and high clock speed ) and it is also computation limited.  What it does not need is a large amount of program memory -- the application will easily fit under the 256k limit.  I just wanted to check that a SPIFI connected memory could be programmed if the actual code remains under the 256k. 

Martin Jay McKee
0 件の賞賛
返信
1 返信

774件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Sat Mar 01 04:38:53 MST 2014
Yes - downloads to such as system is fine as long as the code size is < 256KB.

Regards,
LPCXpresso Support
0 件の賞賛
返信