Does LPCxpresso support other debuggers?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does LPCxpresso support other debuggers?

2,165件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kalpak on Wed Dec 07 23:05:34 MST 2011
Dear All,
Does LPCxpresso support other debuggers like Segger JTAG Debugger?
thanks,
0 件の賞賛
返信
7 返答(返信)

2,145件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by stalisman on Sun Dec 11 03:36:58 MST 2011

Quote: rmteo
:confused: :confused: :confused:
AFAIK, the only low cost development board that has a J-Link included is the FreeScale KwikSitk.




altzhimers is a real bugger on times ...:-)
0 件の賞賛
返信

2,145件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Sal Ammoniac on Sat Dec 10 21:23:50 MST 2011

Quote: stalisman
You seem to be saying that you like LCPXpresso but want to use another tool?

...

It is amazingly decent in fact.


I agree that it's very decent. The only gripe I have is speed when single-stepping code. I use a J-Link on some boards and it will single-step code [I]much[/I] faster than the LPC-Link, which is rather slow.
0 件の賞賛
返信

2,145件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rmteo on Fri Dec 09 08:06:07 MST 2011

Quote: stalisman

A cheap LCP1114 board comes with a [COLOR=Red][U][B]J-Link[/B][/U][/COLOR] included that you can chop off and use for any other more expensive board if you wish.  It isn't JTAG it's 2 wire serial and very useful and practical.

If you compare all the grief of getting to grips with Freescale  products, or even IAR starter kits, to the joy of xpresso, you'll soon  be smellin' the coffee


:confused: :confused: :confused:
AFAIK, the only low cost development board that has a J-Link included is the FreeScale KwikSitk.
0 件の賞賛
返信

2,145件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by stalisman on Fri Dec 09 07:44:34 MST 2011

Quote: kalpak
I was hoping one of the other debugger manufacturers have made a driver/ dll for code red.
The price of code red is very tempting and NXP seems to be rooting for it.
But board manufacturer like Future Designs insist on supplying their development kit with the J Segger debugger.
Hence the query.




You seem to be saying that you like LCPXpresso but want to use another tool?

A cheap LCP1114 board comes with a J-Link included that you can chop off and use for any other more expensive board if you wish.  It isn't JTAG it's 2 wire serial and very useful and practical.

It is amazingly decent in fact.

If you compare all the grief of getting to grips with Freescale products, or even IAR starter kits, to the joy of xpresso, you'll soon be smellin' the coffee   :-)
0 件の賞賛
返信

2,145件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kalpak on Fri Dec 09 06:04:51 MST 2011
I was hoping one of the other debugger manufacturers have made a driver/ dll for code red.
The price of code red is very tempting and NXP seems to be rooting for it.
But board manufacturer like Future Designs insist on supplying their development kit with the J Segger debugger.
Hence the query.
0 件の賞賛
返信

2,144件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rmteo on Thu Dec 08 07:44:25 MST 2011
LPCXpresso (hardware and software) is a closed proprietary system.  I use Rowley CrossWorks which supports J-Link (plus 20 other debuggers including Red Probe and an ARM SIMULATOR as well).  It is a complete C/C++ and assembly code development system for        [B]ARM7[/B], [B]ARM9[/B], [B]XScale[/B], and [B]Cortex[/B] microcontrollers. It supports hundreds of MCUs http://www.rowley.co.uk/arm/Support_Packages.htm
0 件の賞賛
返信

2,144件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Rob65 on Wed Dec 07 23:40:28 MST 2011
I quote from the LPCXpresso product page at Code Red's site:


Quote:
[B][B]Summary of LPCXpresso 4 features[/B][/B]

 
[LIST]
[*]Simplified Eclipse-based Integrated Development Environment.
[*]Device-specific support for a range of NXP LPC family microcontrollers including:
[LIST]
[*]NXP LPC1100 and LPC1200 (Cortex-M0)
[*]NXP LPC1300 (Cortex-M3)
[*]NXP LPC1700 (Cortex-M3)
[*]NXP LPC1800 (Cortex-M3)
[*]NXP LPC4300 (Cortex-M4)
[*]Selected members of the NXP LPC2000 (ARM7TDMI) family
[*]NXP LPC2929 (ARM966)
[*]NXP LPC3130 (ARM926-EJ)
[*]NXP LPC3250 (ARM926-EJ + VFP )
[/LIST]

[*]Wizards to create microcontroller programming frameworks, fast.
[*]Peripherals views of all supported microcontrollers.
[*][COLOR=Red][B]Support for LPC-Link and Red Probe debug emulators.[/B][/COLOR]
[*]No-fuss, single install for complete product.
[*]Available for Windows XP, Windows Vista, and Windows 7 and selected Linux hosts
[/LIST]



LPCXpresso supports the LPC-Link (the debugger on the LPCXpresso module) and Code Red's Red Probe and Red Probe+ debuggers - that's all.

Regards,
[INDENT]Rob
[/INDENT]
0 件の賞賛
返信