Does LPCXpresso support HDK?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does LPCXpresso support HDK?

1,317件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by aferrari on Fri Jul 31 02:08:01 MST 2015
Hello everyone,

I'm using a "LPC4088 QuickStart Board".

Is it possible to use LPCXpresso with mbed HDK system in order to download and debug the software?

Many thanks

Alberto
0 件の賞賛
返信
5 返答(返信)

1,311件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by aferrari on Fri Jul 31 09:22:01 MST 2015
Great job LPCXpresso Support !!!

The mbed serial port driver has fixed the problem.

Thank you very much!
0 件の賞賛
返信

1,311件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Jul 31 06:22:35 MST 2015
If you are using Windows, then I suspect that you may need to install the mbed serial port driver before LPCXpresso will be able to detected the debug probe.

https://developer.mbed.org/handbook/Windows-serial-configuration

Otherwise I suggest you check the documentation for the board for any clues (jumper settings etc).

Regards,
LPCXpresso Support
0 件の賞賛
返信

1,311件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Jul 31 05:39:45 MST 2015
LPCXpresso will automatically detect when a CMSIS-DAP compatible probe is connected.
0 件の賞賛
返信

1,311件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by aferrari on Fri Jul 31 05:05:59 MST 2015
Thanks for the answer.

Now I've connected the board to the PC via USB.

In this way mbed HDK should be used, but when I try to debug the sotware, LPCXpresso is not able to see the card.

Which kind of setting do I have to to do on LPCXpresso in order to use mbed HDK system?
0 件の賞賛
返信

1,311件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Jul 31 02:42:04 MST 2015
The mbed HDK implements CMSIS-DAP. LPCXpresso supports CMSIS-DAP.
0 件の賞賛
返信