Distros that LPCXpresso works

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Distros that LPCXpresso works

1,144件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by renan on Tue Nov 15 16:51:09 MST 2011
Hello,

I have been able to debug using my LPCXpresso 1769 board (OM 13000) with Chakra Linux (an Arch Linux based distro).

If anybody wants, I can provide more info of my system.

I think it would be nice that people using other distros (not the ones officialy supported) post it in one thread.


Thanks
Renan
0 件の賞賛
返信
3 返答(返信)

1,134件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nicolagiacobbe on Mon Dec 05 06:00:19 MST 2011
Using LPCXpresso under Linux.
Ubuntu 10.04 with a core 2 duo PC. At first I had the '57% problem' also but I solved it by changing the USB HUB, now I am using a SITECOM CN-025 and it is working great.
0 件の賞賛
返信

1,134件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by culyun on Sat Dec 03 02:48:49 MST 2011
How did you do it??
0 件の賞賛
返信

1,134件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by FlySnake on Wed Nov 16 15:50:51 MST 2011
openSUSE 11.2 & 11.4 works with some glitches: cannot run debugger more than 1 time in succession - it halts for a 1 minute on 57% and you have to reconnect the board to run debugger again. I'm almost resigned to it and used to reconnect the cable every time I need to run the debugger :)
0 件の賞賛
返信