Designing LPC1769 Based Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Designing LPC1769 Based Board

1,300 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cesimkaol on Thu Feb 07 15:16:48 MST 2013
My microcontroller lecture project is designing very simple LPC 1769   based board in order to learn how to use pcb tools , fabrication and   etc.

There will be only leds and switches. the aim of project is

*How to design pcb for board and how to programming it?

I have to use ISP programmer and Flash Magic...according to my research   on schematics of 1769 based developped board , I should  use P0.2 ,  P0.3  and P2.10 for ISP programmer...

I figure out there will be a max3232 for ttl logic between COM port and 1769 .
TXD0,RXD0 should be connected to T1in and R1out of max3232.But ı cant figure out how ISP's role and where should ı put it...

Thank you for your replies...
0 Kudos
Reply
3 Replies

1,274 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Feb 07 17:14:11 MST 2013

Quote: cesimkaol
... I should design P2.10  pin as a reset button ...While programming Lpc p2.10 pin should be  grounded...



:eek:

-P2.10 as ISP Pin (10k pullup and switch to GND)

-RST_N (Pin 17) as Reset (10k pullup and button to GND)
0 Kudos
Reply

1,274 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cesimkaol on Thu Feb 07 17:03:46 MST 2013
According to information given above , I can directly connect FTDI chip   and LPC's TxD / RxD UART pins(p0.2 and p0.3) and I should design P2.10   pin as a reset button ...While programming Lpc p2.10 pin should be   grounded...

Thank you Zero ...

I will put basic schematic here ...And I want you to examine it pls :)


Thank you for your replies...
0 Kudos
Reply

1,274 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Feb 07 15:51:17 MST 2013
#1 Minimal requirements are TxD / RxD UART connection, ISP switch (= to pull low ISP pin), Reset button :)

#2 I don't understand why you want to use RS232 instead of USB (http://www.flickr.com/photos/58892165@N08/6582736325 , http://www.flickr.com/photos/58892165@N08/6582736169 ) with FTDI (http://www.ftdichip.com/Products/ICs/FT232R.htm)

#3 Instead of adding a serial converter to board I would recommend to use an USB-UART converter (http://www.flickr.com/photos/58892165@N08/6973435771/in/photostream/) and just add a simple TxD / RxD / GND connector to UART :eek:
0 Kudos
Reply