Defining Pin Function in Software

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Defining Pin Function in Software

1,082件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pleonhardt on Sun May 18 11:34:44 MST 2014
I have the LPCXpresso software up and running and am able to run example programs with demo boards.  I am now to the point where I would like to design my own hardware and modify the function of the software.  Can someone tell me where in the firmware libraries the GPIO pin function is set, for example input/output, etc.?  There must be a large table somewhere, but I am not able to find it.

Thanks.
0 件の賞賛
返信
2 返答(返信)

1,074件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Sun May 18 12:19:58 MST 2014

Quote: pleonhardt
I am now to the point where I would like to design my own hardware and modify the function of the software.



Usually UM is including a detailed function description in chapter IOCON  :)
0 件の賞賛
返信

1,074件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by 1234567890 on Sun May 18 11:42:18 MST 2014
Have an intensive look at http://www.lpcware.com/content/nxpfile/lpcopen-platform.
0 件の賞賛
返信