Defining Pin Function in Software

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Defining Pin Function in Software

1,083 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pleonhardt on Sun May 18 11:34:44 MST 2014
I have the LPCXpresso software up and running and am able to run example programs with demo boards.  I am now to the point where I would like to design my own hardware and modify the function of the software.  Can someone tell me where in the firmware libraries the GPIO pin function is set, for example input/output, etc.?  There must be a large table somewhere, but I am not able to find it.

Thanks.
0 Kudos
Reply
2 Replies

1,075 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Sun May 18 12:19:58 MST 2014

Quote: pleonhardt
I am now to the point where I would like to design my own hardware and modify the function of the software.



Usually UM is including a detailed function description in chapter IOCON  :)
0 Kudos
Reply

1,075 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by 1234567890 on Sun May 18 11:42:18 MST 2014
Have an intensive look at http://www.lpcware.com/content/nxpfile/lpcopen-platform.
0 Kudos
Reply