Deep sleep on LPC11U14

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Deep sleep on LPC11U14

549 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Muis on Thu Jan 03 08:52:30 MST 2013
I developed a simple datalogger using the LPC11U24. It records 256 samples per second, and goes to sleep using __WFI(); in between samples. It currently consumes about 2 mA (at 12 Mhz), which seems to match the datasheet.

To further reduce power consumption I'd like to use deep-sleep, and for the LPC1114 there is a perfect example, but for the LPC11U14 there is no 'timed wakeup' example, and since it features a different watchdog (WDT vs WWDT) i cannot port the code easily.

Does someone have a timed wakeup example for the LPC11U14?
0 Kudos
Reply
0 Replies