Debug via the LPC-Link for EA's LPC1788 Developer's Kit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debug via the LPC-Link for EA's LPC1788 Developer's Kit

813件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Thucydides on Wed Feb 08 23:38:01 MST 2012
[B]I tried to debug for the EA's LPC1788 Developer's Kit via the LPC-Link.
I cut the center of an LPCXpresso and I used it as debugger from LPCXpresso IDE ver.4.
But an error [/B]"unable to initialize LPC-Link" [B]was displayed[/B].
How should I solve it? Or there are any causes for the error?
Thanks,
0 件の賞賛
返信
2 返答(返信)

777件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Thucydides on Thu Feb 09 01:22:42 MST 2012
Thanks Zero,
Power is fed by a normal 5V 2A switching DC adapter and the cable is the accessory of EA's LPC1343 quick start board.
Now I succeeded by just changing USB port, strange!
Anyway it seems be OK.
See you
0 件の賞賛
返信

777件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Feb 09 00:36:36 MST 2012
How do you power your EA1788 board? How did you connect LPC-Link and EA1788 board?

They are working together without problems here with 5V power supply and simple 4-wire SWD connection :)
0 件の賞賛
返信