Debug access is blocked

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debug access is blocked

911件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ngoncalves on Thu Oct 13 04:04:49 MST 2011
Hi,

I have an LPCExpresso board with an LPC1769 and I am using it with Code Red under Linux.

After downloading a firmware which probably badly configured the ARM, I cannot enter debug mode or erase the flash.

  I tried triggering the ISP bootloader, has it says herehttp://support.code-red-tech.com/CodeRedWiki/DebugAccessChip, but I don't know where pin RST is located.

  I simply grounded the ISP pin, power-reset the board and then disconnected the ISP pin. It appears that my firmware was not executed, but I still cannot enter the debug mode or change the flash.
0 件の賞賛
返信
2 返答(返信)

902件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ngoncalves on Thu Oct 13 07:47:05 MST 2011
No, I am using Ubuntu. But I finally figured that I had a problem with my code.

I was setting the watchdog, and apparently during debug the watchdog runs independently. So every time I was able to flash the micro, it would block again.

I removed the watchdog code and now grounding the ISP pin, power reset, ungrounding ISP works.
0 件の賞賛
返信

902件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by whitecoe on Thu Oct 13 06:30:07 MST 2011
Which Linux are you using? Not Gentoo is it?

http://knowledgebase.nxp.com/showthread.php?t=2001
0 件の賞賛
返信