Debug Issue: @ startup or IDE reset end up in endless loop at x1fff00d6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debug Issue: @ startup or IDE reset end up in endless loop at x1fff00d6

1,528 Views
jimprince
Contributor I

Debug Issue: No startup or IDE reset end up in endless loop at x1fff00d6.

Using LPC824Max board.

Environment:

Version: LPCXpresso v8.1.4 [Build 606] [2016-03-14]

Operating system: Windows 8.1

VM: Java HotSpot(TM) Client VM (32 bit)

 

This is a "Pro" license: How do I get the promised support that I paid for?

 

What is at x1fff00d6 ?

How do I fix this ?

 

This is a tool issue that is wasting days.

 

Thanks. Jim

0 Kudos
Reply
1 Reply

1,372 Views
lpcxpresso_supp
NXP Employee
NXP Employee

The LPC824 is looping in the bootloader. This means it found no flash image it could boot. Either flash is blank, or, the bootloader couldn't validate the checksum word.

Thanks and regards,

LPCXpresso Support

0 Kudos
Reply