DFU and the JTAG controller...

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DFU and the JTAG controller...

1,202件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by happycube on Tue Dec 08 11:56:23 MST 2009
Can DFU be used again after the LPC-Link firmware is loaded?  I'm considering writing alternate firmware for it (perhaps OpenOCD support?) and being able to reprogram it easily is a huge plus. ;)
0 件の賞賛
返信
2 返答(返信)

1,162件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_USA on Wed Dec 09 18:31:28 MST 2009
Hi happycube,

The LPC-LINK boards distributed embedded in LPCXpresso, can only load DFU firmware from our LPCXpresso IDE partner Code Red. However, the LPCXpresso schematics are posted here: http://www.embeddedartists.com/products/lpcxpresso/lpc1343_xpr.php?tab=res. They are a useful reference for a more flexible LPC3154 design that could accept arbitrary firmware via DFU.
0 件の賞賛
返信

1,162件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_USA on Tue Dec 08 18:45:06 MST 2009
Hi happycube,

The LPC-LINK on the LPCXpresso board is only usable with the LPCXpresso IDE by Code Red. It can be used with other target boards.

-NXP
0 件の賞賛
返信