DALI SDK - for Linux?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DALI SDK - for Linux?

1,766件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sglpc.2015 on Sun Apr 26 01:53:48 MST 2015
I see that DALI SDK 2.0 zip file contains a Windows .exe. Is there a DALI SDK for Linux?
0 件の賞賛
返信
2 返答(返信)

1,476件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Pat on Mon May 04 01:43:08 MST 2015
The DALI SDK2.0 is a self installing .exe for windows. The micro controller sources that are being installed (unzipped) by this file can be used with LPCXPresso under Linux.
Best is to install the SDK on a windows machine and copy the complete installed tree (typically at C:\nxp\lighting\DALI_SDK_v2.0 ) to a Linux host.

This should allow development on a Linux machine.

As background: once installed it provides the following on the windows PC:
-  documentation (application notes, user manual, schematics)
-  example PC GUI to use with the DALI master board. (Using .NET)
-  source code of master and slave microcontroller boards
-  source code of PC GUI

0 件の賞賛
返信

1,476件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sglpc.2015 on Mon Apr 27 21:18:21 MST 2015
Please advise if I should move this query to another forum.
If this is not the right one, which is ?
0 件の賞賛
返信