DALI Master Code for lpc1114

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DALI Master Code for lpc1114

1,798件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by faizal on Fri Jul 01 03:01:49 MST 2011
Hello,

I would like to know if there is any DALI Master example code for lpc1114 ?

Regards,
0 件の賞賛
返信
5 返答(返信)

1,665件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Pat on Tue Feb 19 13:53:49 MST 2013

Quote: kbenni
hello
i use the example to do the dali slave but its working only when its connected to pc with debuggung when i use external power its not working. why???



Which board are you actual using? Are you refering to the board LPC1114 DALI slave board OM13026?
0 件の賞賛
返信

1,665件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kbenni on Sat Mar 10 05:27:34 MST 2012
hello
i use the example to do the dali slave but its working only when its connected to pc with debuggung when i use external power its not working. why???
0 件の賞賛
返信

1,665件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by faizal on Thu Jul 07 06:39:50 MST 2011
Hello,

I modified the code used by LPC2141,so that i can programme it on LPC1114. I dont understand,why the code i've attached in only work using step by step. If i debug it,then i click resume,i dont have the answer(the answer for the command 0xFF97 is 1). But,if i use step by step mode,after the line GPIOSetDir(3,1,1); in function DALI_Init(),then i click resume,i have the answer 1 in hyperterminal. I use the example code uart.c and gpio.c.

Regards,
0 件の賞賛
返信

1,665件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by faizal on Fri Jul 01 04:37:09 MST 2011
Thanks.
0 件の賞賛
返信

1,665件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Fri Jul 01 03:22:56 MST 2011
It's not 1114, but perhaps a point to start :)

LC2141 sample:

http://www.nxp.com/documents/application_note/AN10760.pdf
0 件の賞賛
返信