Could not create the view

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Could not create the view

7,820 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Inclooder on Tue Jun 17 05:40:48 MST 2014
Hello,

I just installed LPCXpresso on my linux (ubuntu 12.04).
I am getting the following errors.

Could not create the view: org.eclipse.wst.server.ui.ServersView
Could not create the view: org.eclipse.datatools.connectivity.DataSourceExplorerNavigator
Could not create the view: org.eclipse.wst.common.snippets.internal.ui.SnippetsView
Could not create the view: org.eclipse.mylyn.tasks.ui.views.tasks

Do I need to install some packages?


Regards
0 Kudos
Reply
2 Replies

6,474 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Inclooder on Tue Jun 17 06:15:27 MST 2014
Hi,

You are right, I used the same directory for Eclipse workspace.

Problems disappear when I hanged it to empty one.

Thank you.

Regards
0 Kudos
Reply

6,474 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Jun 17 06:02:03 MST 2014
Looks like you are trying to use LPCXpresso to open a workspace created by another version of Eclipse. All of those are plugin that are not part of LPCXpresso.

Try opening LPCXpresso on a new, empty workspace.

If you want to use those plugins in Eclipse, you are going to need to download and install them yourself. We are unable to provide any support for LPCXpresso once you have done that.
0 Kudos
Reply