Connecting GPIO to TTL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Connecting GPIO to TTL

899 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fi1953 on Thu Apr 14 02:38:05 MST 2011
If I connect an LPC1114 GPIO  (either as Output or Input) to a TTL gate , do I have to disable the pull-up and/or pull down option of the GPIO  ?
0 项奖励
回复
1 回复

823 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Apr 14 09:00:10 MST 2011
On-chip pull-up/pull-down resistors are weak, so I wouldn't switch them off.

TTL fanout is strong enough to drive them.
0 项奖励
回复