Catch a running system with LPCXpresso?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Catch a running system with LPCXpresso?

686件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by micrio on Sat Dec 01 10:33:33 MST 2012
Can I catch a system without first downloading the code?   My LPCXpresso is listed as a DFU device as expected.   How do I cause the LPCXpresso code to get installed in the DFU and have it stop a target device?

I want to plug into my target device and hit the "suspend" button and be able to look at the state of the machine.   Is this possible?

Thanks,
Pete.
0 件の賞賛
返信
1 返信

680件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Sat Dec 01 11:21:15 MST 2012
Did you read already:

http://www.support.code-red-tech.com/CodeRedWiki/DebugRunningSystem

or

http://knowledgebase.nxp.com/showthread.php?t=2787
0 件の賞賛
返信