Can

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can

719 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rahulvasist on Thu Sep 22 23:43:26 MST 2011
Hi,

I want to connect two LPC1769s using CAN. Is it possible to connect them using cross connections? .i.e. TD1 of one connected to RD1 of the other and vice versa.

Thank You in advance
0 Kudos
Reply
1 Reply

705 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Fri Sep 23 00:08:12 MST 2011
Yes :eek:

See: http://knowledgebase.nxp.com/showthread.php?p=5962
0 Kudos
Reply