Can't build!!!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't build!!!

604件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tom84 on Fri Mar 16 06:59:32 MST 2012
Hey,

i got a problem with my project. I  got a file structure like this:
Project
-> source
          ----> common demo tasks
          ----> FreeRTOS
----      main.c
----      FreeRTOSConfig.h
       .
       .
       .
I can Debug (debug build) without any errors, but when i try to Release (release build). I get the message: "[COLOR=red]error: FreeRTOS.h: No such file or director[/COLOR]"!
The file is in the folder FreeRTOS.....what did i do wrong?
0 件の賞賛
返信
1 返信

587件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Rob65 on Fri Mar 16 12:02:55 MST 2012
you have to create project properties for the release version of the project as well.
Have a look at the project properties and notice that all on the top you can select 'release' or 'debug'. Most likely the project properties for your release project are missing the proper directories for include files and/or libraries.

Rob
0 件の賞賛
返信