Can't activate LPCxpresso IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't activate LPCxpresso IDE

2,215件の閲覧回数
dfae_banchaolan
Contributor I

I got a problem with LPC IDE


- After install, I'was trying to activate IDE by follow these steps.

: Help->Active->Create serial number and register
Then window pop-up noticed "This will overrwrite your existing registration. Continuous?" Then i clicked Yes

: Serial number show up. Then click ok.

pastedImage_1.png

: Then pop-up window show as below. I still click OK

pastedImage_2.png

Then browser notice as below.

pastedImage_3.png

I'm not sure that mistake from my browser or NXP server. but still can't get activate code. Please help me.

タグ(2)
0 件の賞賛
返信
1 返信

1,907件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

I've just checked the LPCXpresso IDE Free activation pages, and they seem to be up and running.

Please make sure you follow the instructions for free activation at:

Activating LPCXpresso Free Edition 

in particular you need to make sure that you are logged into the NXP web system.

Note: MCUXpresso IDE (which superseded LPCXpresso IDE back in March), does not require this activation  process for use in Free Edition mode. So you might want to try that instead. For more details see : http://www.nxp.com/mcuxpresso/ide

Regards,

LPCXpresso IDE Support

0 件の賞賛
返信