Can't Install LPCxpresso on linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't Install LPCxpresso on linux

2,270 Views
alejandrorodri3
Contributor I

Hi, I try to install LPCXPRESSO but I cant. Im already changed the permission but when i execute it nothing happens.

I have:

GNOME Linux 3.16.0-4-amd64 x86_64

Debian 8.6

Notebook:~/Downloads/Installer_LPCXpresso_8.2.2_650_Linux-x86$ ls -l
total 519024
-rwxr-xr-x 1 alejandro alejandro 531465260 Sep 9 04:29 Installer_LPCXpresso_8.2.2_650_Linux-x86

alejandro@Alejandro-Notebook:~/Downloads$ ./Installer_LPCXpresso_8.2.2_650_Linux-x86
alejandro@Alejandro-Notebook:~/Downloads$

Thanks

0 Kudos
Reply
3 Replies

1,673 Views
converse
Senior Contributor V

Have you followed the instructions and installed the required packages? The installer (and the product) will not work without them...

https://community.nxp.com/thread/389036 

0 Kudos
Reply

1,673 Views
alejandrorodri3
Contributor I

Same thing, nothing happens:

alejandro@Alejandro-Notebook:~/Downloads$ sudo ./Installer_LPCXpresso_8.2.2_650_Linux-x86
[sudo] password for alejandro:
alejandro@Alejandro-Notebook:~/Downloads$

0 Kudos
Reply

1,673 Views
converse
Senior Contributor V

Try using sudo

0 Kudos
Reply