Can not reset by pressing RESET button after debug

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can not reset by pressing RESET button after debug

645 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ThanhNguyen on Mon Jul 19 02:47:38 MST 2010
Hi,
I've just started with an simple example that run on LPCXpresso target LPC1768 connected with base board, and worked with LPCXpresso IDE platform.
And I had a confused issue that: when I loaded flash and debugged on LPCXpresso IDE, it could work well. But when I stopped debug and pressed RESET button, the program could not restart until I disconnected power sources and re-connected, it could run in stand-alone mode.
How can I solve this issue because it's so inconvenient to me when i have to disconnect and re-connect power sources many times.

Thanks in advance,
ThanhNguyen
0 Kudos
Reply
1 Reply

633 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Mon Jul 19 04:00:18 MST 2010
I imagine that you need to change the debugger disconnect behaviour. For details please see the knowledgebase entry:

http://lpcxpresso.code-red-tech.com/LPCXpresso/node/43
[login required]

Regards,
CodeRedSupport
0 Kudos
Reply